AXIS#.IL.BW

Description

This parameter sets the current loop bandwidth. The default value is determined by the PWM frequency of the drive and the maximum recommended bandwidth.

The current loop gain AXIS#.IL.KP is calculated as follows:

AXIS#.IL.KP = 2 * pi * AXIS#.MOTOR.LQLL * AXIS#.IL.BW

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kHz

Range

0 to 5

Default Value

Determined by PWM frequency and maximum recommended bandwidth.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.BW

500ah

16h

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5818

1

5818 (0x16ba)

AXIS1.IL.BW

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.BW

5818

Float

Read/Write

-